ControlBuilder wants to hardware download without any change
In One of the project the Controlbuolder wants to hardware download even though there are no difference report . After download, going offline,close the controlbuileder and reopen then it again asking for a downlaod , without any difference report
Answers
It seems some changes made and again that changes deleted. So it seems no difference but actually changes done as per software.
In this case you need to download
by RDPLC Rank: 855 on 1/23/2018 1:57:01 AM | Like (0) | Report
Checking the time stamps should help in identifying where change has occurred.
by rsalles Rank: 10688 on 3/2/2018 4:29:51 PM | Like (0) | Report
Hi, I am with the same problem, but in my case the difference report is pointing to the CI860, and, like you none modification happens. I do the download and if I close the CBM I need download the application again.
Add new comment