Errors registering dll's during installation of Composer 6.1
Installing S+ Engineering Composer Harmony Standalone
Installing to a Windows 7 64 bit environment.
These are the dll's that are not registering during installation.
c:\program files (x86) ABB Symphony Plus\Engineering\Composer Harmony\bin\ComposerConfigDataX.dll
c:\program files (x86) ABB Symphony Plus\Engineering\Composer Harmony\bin\ControllerConfigDataX.dll
c:\program files (x86) ABB Symphony Plus\Engineering\Composer Harmony\bin\ControllerConfigViewX.dll
c:\program files (x86) ABB Symphony Plus\Engineering\Composer Harmony\bin\DataBrowserX.dll
How do I resolve this?
Answers
Hi:
Did you try registering the files manually?
the command line is Regsvr32 /s "Path of the file"
BR
Add new comment