COMMUNICATION PROBLEM WITH WINDOWS 7 ( HOME BASIC )
Dear sir,
I have PC with windows 7 Home basic operating system , also I have TK 503
communication cable with installed driver in my PC , but the problem is no communication held in between PC and PLC , so please tell me proper way
to communicate PC and PLC.
Thanks & Regard
SAGAR
Answers
Hi
Before you can use the TK503/TK504 programming cables, the appropriate USB driver must be installed on your PC or laptop.
The driver for the TK503/TK504 programming cables are installed in two steps:
Pre-installation of the drivers on your PC using the program TK503&TK504Installer.exe.
Installation of the new hardware in Windows after the TK503 programming cable or TK504 programming cable is plugged in for the first time.
Reference Link:
Search ABB Library for "Programming Cables TK503/TK504"
Best Regards
Sunny Khatri
Add new comment