Upload the program from PM864 Controller Using Control Builder
Is there any possibility to upload application program from PM864 or PM861 Controller using control builder from any PC Which having installed control builder.
in case i dont have application program backup & i want to upload program from controller.
if possible then how to upload?
Answers
NO
Dont loose the source code. If you're concerned this could happen, save it in a CF card in the controller. (or SD card on PM891 )
Hi
Some following points to consider:
- There is no possibility to upload from any controller to PC.
- For Backup, These application are strored in Aspect Directory Backup or you can selectively take Control Structure Backup (Respective Control Network).
Best Regards
Sunny Khatri
Add new comment