Issues in configuring SignalAE block from Alarm and Event Library; -30 in the AIStatus?
I was facing issues in configuring the SignalAE block from the Alarm and Event Library. I am using it in some custom logic and I believe I have configured all the parameters correctly .
But after going online, I keeping getting -30 in the AIStatus parameter . I believe there is some issue with the SrcName that the block SignalAE requires from the object it is being intiated in.
The Help is not very clear and says: 'SignalAE does not have a SourceName Paramter, instead a parameter called Name must be defined in the object where SignalAE (??).'
Also please elaborate on the role of the Parameter "Message" in the block?
Please guide as to what i maybe doing wrong?
Voted best answer
Hello,
Check if the name and description has spaces or a not allowed character.
Regards
Add new comment