Delete old systems on EW
Hello!
I have a standard system: AS, CS, EW with redundant RNRP.
Old systems stayed in system status viewer and "workplace" launcher on EW after backup recovery (to be honest, I just forgot to disconnect EW with "update node" before delete the old system on CS and AS). Backup system works well.
I just want to get rid of this dead systems in the list.
Someone know how to do it?
Thanks in advance!
Voted best answer
You can also do a cleanup in registry. Your systems can be found under HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\ABB\AFW\Systems or under HKEY_LOCAL_MACHINE\SOFTWARE\ABB\AFW\Systems on a 32-bit platform. Don't remove {FFFFFFFF-FFFF-FFFF-FFFF-FFFFFFFFFFFF} or your active system.
Answers
Hi Alexander
I would do the following,
using Configuration Wizard on EW:
1) Disconnect Client EW from system(s).
2) Delete System(s) on EW.
using Engineering Workplace on primary AS:
a) Navigate to Node Administration Structure
b) Locate EW:Node Definition aspect
c) Connect remote node
BR Carsten
I would do the following,
using Configuration Wizard on EW:
1) Disconnect Client EW from system(s).
2) Delete System(s) on EW.
using Engineering Workplace on primary AS:
a) Navigate to Node Administration Structure
b) Locate EW:Node Definition aspect
c) Connect remote node
BR Carsten
Source:
Add new comment