AC500 CodeSys Timers not working
I made a logic in Codesys FBD with several timers for different motors. The timers in first 10 rungs of the POU are working, rest of the Timers arent working. I have checked decleration for all timers & found all to be same with different names. I used all TON timers. Then why only 10% of the timers are working & rest 90% are not working. Is there any way to get the rest of the timers working. I face alot of pressure at site. I will be grateful if anybody could help me As soon as possible. PM573-ETH AC500
Answers
Could you please share with us the backup of your program or export of your POU?
So we can have deep idea about your problem.
Add new comment