ISO on TCP Protocol
Hi Stefan
There is a mobile machine (Stacker/reclaimer) with siemens controller. The supplier mentione the protocol is ISO on TCP.
- How we can integrate this kind of protocol to the AC800M?
- What kind of cummunication interface we need on aC800M side?
Best Regards
Yousef
Answers
Controller-to-controller communication can be made in many different ways.
Have a look at Profibus (CI854), Modbus (serial or TCP/IP based using CI867) and the Siemens 3964R serial protocol.
Serial communication based Modbus and Siemens 3964 should be possible to use w/o additional hardware since most controllers come with two serial ports (COM3 and COM4). Additional serial ports can be added using CI853 units.
Add new comment