I want to creat panel layout aspect in workplace structure, not in library structure and disable graphic toolbar
Hi mr Stefan!
- I created 1 workplace for operator. When i configured application bar and workplace layout, i had 1 problem. When i creat new aspect for panel layout. I could not find panel layout in aspect list. but i could see it in old workplace. and i also created and found it easily in library structure. So my question is how to creat layout aspect in workplace structure without copy from old workplace?
- in operator graphic, how can i delete or disable area icon in top toolbar? Because i dont want operator can navigate to other graphic in area. I can creat for 1 graphic with 1 area. But it make me more time. so i dont want to do that way.
Thanks so much!
Answers
Originally in the early days of 800xA, all panels where located in the Library Structure - often only one panel was used "StartupDisplayPanelLayout"
With multiscreen and tabbed navigation a need for more panels have developed. Some may have elected to copy the panels from their original location over to the Workplace Structure (where they actually are called from). I suspect the (old) aspect rules have been set so that you are not permitted to create panels in the workplace structure, but I suspect you can copy them there.
The icon you want to remove is part of the Standard Tools of the Standard Frame used by a process graphic. With some effort, you could create yourself a new customized frame where the tools are configured differently, e.g. no Object Icon tool. Changing the Standard Frame would also change a large number of diffenenty types windows in 800xA making use of the same frame. Frames are decided by the View Class, so you might have to spawn a new View Class as well. Not a simple task...
/Stefan
Add new comment