Smart Client 2.2 RevC RU2b on 800xA 6.0.3
Hi,
I have DP installed on Connectivity server and SC server on a webserver. Property browser is working correctly. Problem is with graphic browser I can't see the System. I can't see any errors at c:\abblogs. Find attached screenshots from Program supervision manager.
Thanks for your attention. I'm looking forward to your reply
BR,
Miro Proleta
Voted best answer
Miro,
As said before, I believe it may be time to open a Support Case. However there are a couple of procedures that you can do to either examine yourself or send the information with your request for a Support Case. There are two places that can be set to enhance the output of messages in the system that may point to your issue. I have attached two procedures that will allow you to gather this information.
Let me know if this helps.
Regards,
Geof
Answers
Miro,
For my test system, this is a singlenode system, therefore all the Data Providers are installed on the same node, ie. the SC Server & DP entries. However, the concept is the same, the "- server" argument in the providers on the DP node should have the IP address of the SC Server.
Regards,
Geof Ledin
Miro,
I would suggest opening a Support case with your local RAC and sending the C:\abblog files from both the DP node and the SC Server node,(each has their own). You can also export the entire setup of the Data Providers as they are stored in the MS Registry on both nodes. This may also help, see the attachment for procedure.
Regards,
Geof
I found the solution, .NET Framework 3.5 was not correctly installed.
I can see the display in the graphic browser. But now I have another problem, after application is started I can open only first display that I chose. When I open second display or any other display after first i get empty display.
BR,
Miro
Add new comment