SMS and Email messaging
I am setting up an Email messaging service and have figured out everything excaept the SMPT settings. Can someone please explain what is needed here?
Alos, is it OK to just type an email adress and not use an email program like outlook?
Answers
If you talk about the Settings in the "Email Device" Aspect, there is almost no configuration needed there actually.
What you need to have installed on the Server node is an SMTP Relay (Windows Features - "SMTP Server") and it needs to be configured to forward Mail from Localhost to your actual EMail Server - note that this requires working Internet Access and DNS Settings etc.
Check the 800xA Configuration Manual 3BDS011222 for the Description.
by Sumit Gargav
which system ? AC500, 800xA, compact ?
by IEFIOSU Rank: 798 on 1/30/2015 1:30:04 AM | Like (0) | Report
sorry, its 800xA SV5.1, not sure if its FP or not
Add new comment