OPC server not showing connected controllers
Dear
My OPC server pop up is not showing the connected controllers,what should i do?Please check the image attached. Controller is PM590-ETH,Control bulder version is 2.2.0
thank you
Answers
The first image looks very similar to the AC 800M OPC Server panel...
... but the second image is very far from anything I've come across with AC 800M.
Are you really using the correct OPC server for the PM590?
Hi,
As Stefan advised, the AC800M OPC server is for AC800M controllers.
For AC500 you should use the following OPC Server (Named CODESYS OPC Server or similar):
Add new comment