How to connect AC31 with CP430C-ETH through Modbus RS232?
Hi guys,
I'd like to connect AC31 07KT98 with CP430C-ETH through RS232 but I cannot. I don't know which Controller I should choose in CP400 Soft because there is no AC31 PLC. I tried some AC500 types and Modbus Slave and so on but without any success. Could you help me? Thanks
Answers
It's OK now with older version (1.0.2) of CP400Soft. I don't understand why, but in newer version (1.3.0) AC31 is missing!!! And another thing is that the version 1.0.2 isn't compatible with 64bit version of Win so the compiler doesn't compile the project. Anyway you can download it to the panel but communication with PLC doesn't work. So be careful!
Add new comment