pm571-eth programming assistance
I need help connecting to and programming a pm 571-eth PLC.
I am using control builder plus V2.1.0 but that does not allow you to target the 571-eth plc and as such i am having a hard time programming it.
I have had limited success programming directly from CoDeSys V 2.3.9.46 which allows you to target a pm 571 PLC but not with a ethernet connection also. This allows me to upload a program directly via a TK503 serial to usb cable, however has a configuration fault because the ethernet connection is not included.
Can anyone give me some help on how to connect properly to the plc!
Answers
There is nice videos on YouTube for beginners... Try to check all, for your case can be suitable next:
https://www.youtube.com/watch?v=L0HhKEg7vEI
Hope this helps...
brought new thread text here.
"pm571-eth programming
How do you connect to the pm571-eth in control builder plus v2.0.2 if it is not in the target list or have a template file?"
From Ross, (Pls continue in same thread for better continuity - admin )
"pm571-eth programming
How do you connect to the pm571-eth in control builder plus v2.0.2 if it is not in the target list or have a template file?"
From Ross, (Pls continue in same thread for better continuity - admin )
Add new comment