motor start and stop in E1 with level logic,but motor stops manually and agian changing E1mode mot is not starting
i created one mot1 block with level logic hig and low,it is running in e1 mode but if stopping manual again putting e1 mode even level is high motor is not starting,
Answers
Dear Rajan, pls continue in same thread, even though it's closed related users get notification on new answer or comment added to this thread. added newly posted question text here.
- Admin
"we created level logic in pm891 controller ,problem motor taken in to manual again putting e1 is not strating
in pm 891 controller we made level logic high and low limit it is running ok in e1 mode. if stopping manual again change to e1 even level high and e1 bit also true but motor is not strating "
From Rajan,
Add new comment