abb plc pm572 and ethernet module cm572 confıguration error. Connectıon through tk503 cable.
I have 1 PM572(TK503 CABLE CONNECTION) plc, 3 DO562, 3 DI562 modules, 1 CM579 PNIO communication module. The problem I face here, after confıgurıng my project in automation builder v1.2 through CoDeSys when I try to login I get error confıguration problem. I have tried every thing like, changing comunication module and cpu respectively but all in vane. I also formated my pc and again install automation builder but didn't get any positive results.
Did anybody face the same problem or have any solution/advice?
Did anybody face the same problem or have any solution/advice?
Answers
Hi Faris
your problem may have originated from multiple causes ...first of all make sure that your Automation Buider session have correct define the communication parameters.
Do not forget that your domain / subnetmask and IP adress of PLC must be the same of PC - network where you should activate the project.
In the attached image one simple configuration in AB. The only difference I used in my project PM573 ETH.
For serial communication with TK cable, you must use com_param settings as the other attached file
Of course in Codesys the parameter are the same.
Hope this help you
Plc configuration error picture and plc project picture are attached.
Add new comment