Recommended Thin clients for 800xA Virtualization
Hi all
Is there an updated list for recommended hardware thin clients?
I found only the file "9AKK105713A9849_F_Session_6_Virtualization.pdf / © ABB Inc 3BSE074389 en. October 29, 2013 | Slide 14".
And there is written that the recommended hardware would be the HP T610 and a Dell solution is in progress but not certified.
Updated information would be very usefull.
Thanks!
Voted best answer
I've used T610 and T620 with 800xA. But I can't really imagine why another solution as long it's MS Windows based wouldn't work as the only thing the thin client has to do is to provide the remote desktop programm.
But an official ABB source would be nice as this is my personal opinion as an engineer.
Answers
The other question is:
Is the HP T610 one and only thin Client that ABB recommands?
Or can I use for example a thin client from Dell or Lenovo to get the same result?
I'm looking at the moment for a thin client with support for 4 monitors and a fanless design.
The HP T620 looks like the right solution... but I don't know if ABB would recommand it.
There are fanless thin clients from Dell too. The Dell thin clients have the same specs and OS like the clients from HP.
And I can't find any news about the "Dell solution that is in progress since october 2013"
Add new comment