MY ENGINEERING STATION REPORTS IN VIEW OF WINDOWS EVENTS, ERRORS WITH "TMSYNC.EXE" ORIGINATED BY FREELANCE 2016 SP1
MY ENGINEERING STATION REPORTS IN VIEW OF WINDOWS EVENTS, ERRORS WITH "TMSYNC.EXE" ORIGINATED BY FREELANCE 2016 SP1. HOW CAN I CORRECT THIS PROBLEM?
Answers
Hi hgarcia,
This may be caused by many different factors.
Do You observe time synchronization on Your Engineering Station?
Which version of Freelance and Windows systems are You using?
What type of user account have You configured for Engineering user?
What UAC settings do You have in Windows?
Do you have proper IP settings (address, mask, etc.) and is it in standard Freelance subnet?
Normally tiem sync works fine (assuming it is enabled) on standard Freelance network (172.16.1.x with 255.255.240.0 mask) with disabled UAC and administrator account but in newer versions (2016SP1) there where some changes to how the accounts should be configured (it was connected with UAC compatibility). You can check the Release Notes for details.
Hope this helps,
Mike
Hello hgarcia!
Has your problem been solved?
comes upon event log -
URcvError: 00000522H in TMSYNC.d CGENLIB - Windows 10.
Freelance 2016 SP1 RU2
522H - This error on google says User Rights. This Is just an Operator Station.
by JuergenV Rank: 73 on 1/10/2018 5:18:42 AM | Like (0) | Report
What message exactly?
Add new comment