IAC variable error in controller log file?
What is the meaning of error "IACInVariable::VerifySequenceNumber First fault - degraded sequence number Diff: -7437887" in controller log?
Only the numeric value indicated above is different is some cases. However the message is the same.
Answers
Hello,
which version of system you are using?
check name in both source & destination controller should be same.
ensure both controllers are downloaded? This is the case when you have added the variable in source & not added in destination somay be variable is unresolved.
Add new comment