SFC Viewer Settings
I've built a sequence with Function Designer. I've made all the steps with arbitary names like Step2, Step3 etc. When I open the SFC Viewer I only get step names for each action. Is there any setting so that I can show Step description texts along with the names?
I thought the SFC Mapper could be used maybe to add a step information to each step but does that have connection to the SFC viewer?
Can I add a new Property Translation Extended aspect to be able to write step information to each step?
I could of course build a new display and adding the SFC viewer and add texts along with each step but that's not the solution I want to use as it won't be that flexible.
Answers
We've build a custom Control Module Type which we connect to the SFC.
This CMT uses Property Translations to write step information for each step.
We tend not to use the SFC Viewer because it is difficult to read for non programmers.
by admin Rank: 46 on 12/17/2013 1:15:14 AM | Like (0) | Report
hello,
Does previous question answers this question, too ? http://www402.abbext.com/What-ConfigDataForSFC-setting-do-q134789.aspx
by Anders Bergvall Rank: 1332 on 12/17/2013 3:12:35 AM | Like (0) | Report
Mabye, I haven't been able to test the suggested sittings in this other thread. I may be so that the variable description shows up if I fix this feature pack.
Add new comment