PLC Connect Modbus TCP/IP to AC500
Hi
I have to connect to a AC500 with PLC connect.
In PLC Connect the IP adress Port and MODBUS Id must be edited.
My question is want is the MODBUS Id of the Ac500, internal Modbus TCP/IP
regards
Henning
Answers
Hello Henning.
The Unit ID is usually 0
When communicating AC500 to AC500 it is 0.
BR
Gustav
Add new comment