Reading bulk data of 800xA through excel
Dear team,
I am trying to get bulk data of 800xA into excel file, but I have failed.
Could anybody give me advised for this?
Current status is that
1. Bulk data cannot be uploaded to excel.
2. Seems additional setting is required in "Add-in" in excel, but nothing can be handled related to bulk data.
Sorry for weak explanation.
Thanks.
Best regards, JS Choi
Answers
Hi,
You have to add BDM as add-in excel. then you will get the all BDM option.
To add the BDM features to Excel, you will need to go to the "Add-Ins" section of the Excel Options and select at a minimum the four COM Add-Ins as shown to the Active Application Add-Ins.
Regards,
Geof Ledin
US-OCS-SL-L3
by rahilmohammed Rank: 59 on 12/27/2017 4:41:28 AM | Like (0) | Report
Hi,
Answer by jungleras in the below link may help.
http://www402.abbext.com/Bulk-Data-Manager-BDM-won-launch-EXCEL-2013-800XA-V6-Win-81-q2124794.aspx#commentsList2133596
Add new comment