Freelance 2013 SP1 - DO828 output mapping byte swop ?
Hello has anyone experienced this using Freelance 2013 SP1 with DTM for DO828. When the output for channel 16 is driven HIGH, the actual output channel 8 is activated?
It seems as though there is a byte swop?
Answers
Hello,
Am able to find one field alert
Hi,
Refer the attached memory map details of DO828 module. For freelance, S800 IO modules template(pre-configured) are available in App section. You can download and use it.
by LJohnson1 Rank: 459 on 1/5/2015 3:02:33 AM | Like (0) | Report
Hello, thanks for the feedback however this bulletin refers to the DO818 not DO828 and also discusses OSP using AC800M. I am looking for info when using Freelance without OSP
Add new comment