Freelance 2013 SP1 - DO828 output mapping?
Hello, has anyone experienced an issue with the outputs being swopped on the DO828 for example when channel 16 is driven TRUE, output for channel 8 is switched ON ?
We are using the latest DTM.
Answers
Hi,
As per answer to same previous post, There is issue with OSP value using DO828 via DTM in CBM, That bytes are swapped and for that work arounds are described in that product bulletin.
But what you have described in in question text is different from above case, that not for safety values but seems there is byte swap at main values. Will check for if there is any bulletin for freelance and try to get information. But as work around try table below and connect your channels accordingly to get correct bit at correct channel. check if that works and feedback if not.
I propose to use S800I/O templates using GSD, that should work perfect. check associated app here.
Add new comment