Connecting AC800M to Panel 800 ?!
Hello All
i have AC800M plc and i want to connect it with ABB Panel 800 and this is my first project on ABB so please any one know answer me as soon as possible ?!
Thanks all
Answers
Greetings,
There is an manual abaout Panel 800 Programming and Installation. Please see below link
http://www05.abb.com/global/scot/scot400.nsf/veritydisplay/c6f41b4bfddf2ca0c125
7c06002b85da/$file/3BSE069489-601_-_en_Panel_800_Version_6_Panel_Builder_Progra
mming_and_Installation_6.0-1.pdf
Communicating the Panel with AC800M Controller is explained on Section5.
Hope this helps you.
Hi,
Two modes of communication are mainly used.
1. Through Ethernet
2. Through profibus.
Through Ethernet:
No additional hardware is required.
Process panel and controller shall be in same control network.
Define the variables in access variables. These can be accesses in process panel.
In peripherals of process panel, select ABB control network.
Through profibus:
CI854 on controller side and CB801 on process panel sideneeds to be considered.
In peripherals of processpanel, select Profibus 'Profibus DP'
If you have any specific questions let me know.
Cheers.
Add new comment