Is it possible to upload AC31 07KT94 program(IL) to AC500
Is it possible to upload AC31 07KT94 program(IL) to AC500 using any tools ?
Answers
It is many times discussed that issue. I don't know any tool for convert of AC31 program to Ac500, either I think upload of program is not possible. You need to have a source code (the project loaded in the PLC) in order to go online.
http://www402.abbext.com/advant-controller-31-program-uploading-q12282802.aspx
Well if you have the IL source code you can convert it to AC500 IL or maybe structured text with the help of a generic programming language c++, or VBA in excel etc. Large parts of the IL will be binary logic which will be easy to convert. We have done such a conversion from AC31 to AC500 IL and that works pretty well as IL is a simple language with not so much commands.
Add new comment