High Speed Counter
Please help me to find out solution.
How can I use DI524 as a "High Speed Counter", or is there any module available? like DC541?
Answers
Yes, you have I24 and I25 - two channels, that you can use as fast counters with DI524 only with AC500 CPU.
Please refer help files, AC500 example projects, also this post could help:
http://www402.abbext.com/Counting-pulses-digital-input-q12206426.aspx#commentsL
ist12215419
Hi
in addition to the good answer of kstoilov, you can find one example and more information at the follow link:
http://search-ext.abb.com/library/Dow...
Hope this help you
Add new comment