3th Party Profinet I/O to 800M Controller
Hi
I should link Siemens Profinet I/O's to 800M Cpntroller CI871K
Is there a "hwo to do.." for that?
Whats neede from ABB scope?
Whats needed from Siemens (GSD's..)?
How time consuming is it?
Thanks for your tips and triks
Voted best answer
The AC 800M does indeed support PROFINET IO. This support was added in version 5.1, released year 2010.
The CI871 Communication Interface makes it possible for an AC 800M Controller to be connected to a PROFINET IO network. This is achieved using the PROFINET IO hardware library (CI871PROFINETHwLib). The Device Import Wizard included in Control Builder can be used to import third party definition files (*.gsdml) for PROFINET IO. CI871 has no support for redundancy.
Read more in the user manual “3BDS021515-510 A, AC 800M, PROFINET IO, Configuration”.
Answers
Hi Rudolf,
I am not an expert of AC 800M and profinet, but I have heard about ac 800m supports profinet I/O. check manual 3BDS021515-510 A, attached here with image of ac 800m + profinet I/O. lets wait for some SME opinion here.
by Rudolf Huber Rank: 885 on 12/10/2013 5:20:12 AM | Like (0) | Report
Hello Hans. Thanks for your answer.
Yes, I knew the CI871 Communication Interface makes it possible for an AC 800M Controller to be connected to a PROFINET IO network. Does the the PROFINET IO hardware library (CI871PROFINETHwLib). and the Device Import Wizard in Control Builder include third party definition files? (*.gsdml) Are there ABB tested files for thyrd party Profinet I/O's ?
Or do we need to get the *.gsdml files from thyrd party?
What has to be verified concerning Verion compatibility?
by hryaomr Rank: 7094 on 10/20/2015 4:56:22 AM | Like (0) | Report
I have the same problem connecting Siemens CP343-1 Adv to CI871. GSD file is imported,CI971 Name,Profinet Station Name, device IP (Profinet) are set properly, according the naming rules, the link is established, but there is no communication - IO connection error. From WEBserver, I see that the Profinet station is OK
Add new comment