running job object
By mistake one of our customer has deleted Running Job object in Scheduling structure.
I dont have structure backup of Scheduling structure.
Is it possible to restore RUNNING JOB object through Maintenance Backup.
How can i restore?
Voted best answer
Running jobs Object can be imported from the following file location
C:\Program Files (x86)\ABB Industrial IT\Inform IT\Scheduller\Import\2_Scheduling Object.
After opening that afw file only inport Running Jobs.
Answers
No, Its not possible.
If you import the running job object from the maintanance backup then it will import the GUID like {abcegd----------} instead exact object name as Running Object.
Alternate solution:
But still you can get this by restoring the backup in temp. station & export the running job object only & import the same to your running system.
Add new comment