ABB PM573 PLC-AX561 error
ABB PM573 PLC we are using in our system, Program in run mode, One AX561 is showing Power on(Green light),Below (red light)Error, and other Digital card also showing DX561,DC523 bottom showing ch-err (red light)
Guide me.
Answers
Hi
to have an overview of the error indicated, you need to connect PC to PLC using Automation Builder and investigate the error that the cpu give you. In function of the type of error, the help file guide you to solve.
IMHO probably the error could be originated from I/O bad connections or moisture/dust in connection terminals, or open wire connection.
Hope this help you
to have an overview of the error indicated, you need to connect PC to PLC using Automation Builder and investigate the error that the cpu give you. In function of the type of error, the help file guide you to solve.
IMHO probably the error could be originated from I/O bad connections or moisture/dust in connection terminals, or open wire connection.
Hope this help you
Add new comment