Compact 800
What is the difference between remote client and client in compact 800?
Voted best answer
Remote client enables access to Copmact HMI from a standard workstation (no ABB software installed) over plant network. You will require a remote client server (in addition to compact HMI server) and multiple PCs (standard PC with no ABB software installed over plant network) can access real time information. The remote client description is provided in product guide on page 51 & 52. Normally, a project will require normal client (not remote client) only.
Refer to manual- 3BSE041037-510 compact HMI 800 V5.1
Add new comment