Freelance Digivis Graphic libraries ???!!!!
Hello,
What is the solution to update the Digivis graphics to have predefiened libraries such as 800xa symboles or SIEMENS Wincc symboles?????
Regards
Voted best answer
Hi,
Freelance is having rich default macro libraries that you can find at macros folder and from FGR design page you can upload that from C:\Program Files\ABB Industrial IT\Freelance\macros, e.g go to FGR config page and follow screenshot below
I do not have idea with 800xA and Siemens Wincc symbols and not aware if there is such predefined libraries exist to update. Interesting to know if someone is using that.
Source:
Answers
The graphic macros libraries can be easily updated. In example the macro classes can edited. If a newer version of a macro class should be available, the class can be replaced in CBF project tree.
by REFA Rank: 102 on 3/18/2013 1:08:26 AM | Like (0) | Report
ok!
Add new comment