Danfoss FC302 Profinet
Hello! I have problems with the profinet comunication to Danfoss VLT FC302.
I have configured the module in Control Builder with the latest version of GSDML file (GSDML-V2.31-Danfoss-20160616). The Profinet name and Ethernet parameters (IP, mask, etc.) was right asigned.
However, the frequency converter says "wrong configuration". Its receives correctly the control word and frequency setpoint, but in the plc I cant read the status word.
Please, see the attached file with error information in Control Builder.
I have tested with several telegrams (PPO) but with the same result.
This is the version information for Control Builder.
Product: ABB Control Builder M Professional 6.0.0
Version: 6.0.0/1
Build: 6.0.100.27
Please, tell me if you need some extra information. Regards!Answers
This question has not yet been answered.
Add new comment