Deleting Function Blocks in CBM that are inserted into Functional Structure
I have some auxiliary equipment controlled by AC800M on an 800xA System used for Power Distribution with IEC61850 Connect. To be able to consolidate the Alarm Lists for the different Substations the only possibility i found is to have the AC800M Controller Objects in Functional Structure together with the IEC61850 Objects - this is possible manually by Context Menu "Insert Object..."
However in this configuration deleting any Block in the Control Application is not possible anymore - this means that editing a Program in Control Builder will fail if any Function Block is deleted with the following Message:
[Error] Delete operation is cancelled, the object 'MyFunctionBlock' is linked into another structure!
[Notification] Refreshing application: N01
Transaction Cancelled.
Does anyone know of an Option that tells Control Builder M to anyway delete the Object even if Inserted to Functional Structure or some other workaround for this error?
Answers
There are two ways to delete function block.
You need to delete from engineering workplace.
1) Delete the function block from all the structures except controll structure first then delete it from control structure.
2) Goto control structure -- function block -- delete the aspect called "Function structure" then delete function block object.
I think it should be deleted from Functional Structure:
Try this: Right click on the object to be deleted -- > Advanced --> Delete from all structures.
Hope this will delete the object from the linked structures too..
Add new comment