Datadirect for AE - No Aspect to select
Hello guys, I am needing to find the solution to the problem with the DataDirect for AE. Everything works normally, but at all times I try to perform a query DataDirect aspects do not appear on the right side. No structure presents aspects alarm / event. I've checked the IM settings, username and password AID. The problem occurs on all users of the system as an example 800xAService and Engineering. Someone already saw similar problem? Any idea to help?
System SV 5.1 FP4 RevD
Regards
Marcelo Scarillo
Answers
Hi! I think that the problem is because, as i seen in the image, you don´t have a system connected to the excel file. Try that...see the atached file. Good luck!

Add new comment