BC810 online replacement
Hi
Is it possible to online replacement of BC810 module in redundant system or not?
if yes, is there any procedure for replacement?
Finally is there any document that mentioned this feature?
Voted best answer
Hello,
Hot-swap of BC810 is not possible.Please refer the attached image
Page no.99
Answers
Hello,
BC810 is a bus coupler which has introduced to ensure controllers can be replaced online with baseplate without disturbing the plant process & to ensure cross communication when ex: upper controller down & lower Red.CEX modules down then Lower controller & upper Red. Modules still run through BC810 & vice-versa.
Its not recommended remove the BC810 when the process is on line.
Add new comment