What is the main Differance between Drive window and drive window light
Greetings
What is the main differance between Drive window and Drive window light software?
Is thier is any extra options in the full version?
Regards
Voted best answer
DriveWindow Light connected to the drive though slow RS-232 interface while DriveWindow uses high-speed DDCS link (allowing to connect to the multidrive system such as ACS6000, but require special optical adapter such as RUSB). And with the DriveWindow it is possible to make a complete drive backup (system software). DriveWindow Light can only backup a drive parameters. That's the main difference I think...
Refer to the 3BFE 64560981 - DriveWindow 2 User's Manual and 3AFE 64560913 - DriveWindow Light 2 User's Guide for more details.
Answers
Difference between Drive Window & Drive Window Light.
Drive Window - DDCS Protocol (Fiber Optic Communication) based Tool. - Used to do Commissionining of LV Drives Like ACS600, ACS800 & DC Drives Like DCS600, DCS800 and MV Drives like ACS6000, ACS1000 etc. - More Faster signal updation & Trending.
Drive Window Light - RS232, 485 Communication based Tool. - Used to do commissinoning of LV Drives Like ACS140, ACS160, ACS350, ACS400 ACS550 & ACH550 and DC Drives like DCS800. And also can be used to commission LV Drives Like ACS600 & ACS800 (Only Standard Firmware & Pump Fan Control Firmware)
Add new comment