Maximum I/O's AC500 PLC can handle?
What is the maximum I/O's ABB AC500 PLC can handle. What is the configuration to achieve the same. Please reply. Thanks in advance .
Reg,
Gaudham.V
Answers
This answer copied here from previous duplicate thread answer by erik,
central I/O: DI 224, DO 168, AI 64, AO 64
max 4 comm modules + CPU + 7 modules(max 4 analog) + FBP-Interfacemodule + 7 modules(max 4 analog) see AC500.gif
decentral/remote I/O depends on fieldbus (max 4 comm modules)
/Erik
The maximum that my team has attempted to configure before is 80,000 digital I/O points using PROFINET I/O at 1000 ms cycle time.
RoyChai
what was your configuration (CPU, communication modules, PROFINET IO slaves)? What kind of HMI have you used and what was HMI-PLC communication cycle?
by admin Rank: 37 on 12/6/2014 3:51:42 AM | Like (0) | Report
Dear Gautham,
Please avoid using duplicate threads by duplicate id's. also deleting your duplicate id. Using single user id will help you earning more points and you can redeem earn points now.
Thanks for your understanding.
Cheers
-Admin
Add new comment