Codesys opc server v3 in simulation mode
I have configured opc server v3 with simulation mode and using C:/..../project.sdb for symbol file. I'm using control builder plus 2.2.
For watch the opc values I'm using matrikon opc explorer.
The problem is that the values doesnt change when I force/write values in codesys v2.3.
I mean, I login/run codesys in simulation mode and I force/write some values, after that I watch the opc explorer window and the value tag I added doesnt change. Is like codesys is not linked with the opc server.
What should be the configuration in codesys in "Communication parameters" ??
Or what configuration I need to do in order to get the opc values tag updated?
Thanks.
Answers
I have received an example from, plc.support@de.abb.com. Please find the attached one.
Source:
Hello Scarebyte,
To avoid duplication on topic merged new question related to same thread here.
Recommended to follow same/one thread on same topic. Keep sharing...
Cheers
-Admin
Add new comment