AC800F Different Time Zone Error
I have built an project with Freelance2013(Controller AC800F Redundant system)
I import my previous export, when ı try to download ı got a warning with different time zone then can not download with the following error
"Industrial IT System Bus Connection
BootStrap not possible E_COM_BOOT_CONFIG_TOO_MUCH_PRAM_ERROR"
I achieve to make system run with building a new project but ı need this import so much.
I have tried everything about changing timezone
Urgent help is needed
Thanks.
Voted best answer
Hi,
Even with different timezone one can download to controller say no to popup appears while download with different timezone.
but here from error message seems it's not related to timezone but something related to PRAM - memory. please check the controller type of AC 800F i.e PM802 or PM803, in configuration and physical hardware is matching ?, because incase your are trying to download AC800F(PM803)16mb to AC800F(PM802)4mb the configuration may not fit and you may get such error.
So in CBF check AC800F type and also check on AC800F physical hw side plates there is sticker you can find controller type. it should match. hope that helps pls revert back with more details if not resolved.
Answers
Follow the screen shot for changing the time Zone-
hope this will help
Sumit Gargav,
The point that you mention about PRAM is correct
My CPU is 802F and ı use 9.2 version. When you change from default 803F CPU type to 802F PRAM and Number of objects stays same which blocks you to download
Another PC ı build my project with Freelance 2013. 2013 version automatically adjust PRAM size and Number of objects. I realize this and change these values manually in 9.2 version of Freelance. That costs me sleepless 27 hours.
Add new comment