Composer Harmony 6.1 Installation issue
While Instaling S+ Engineering Composer Harmony 6.1.0.27 , the following .dll files are not getting registered under following installation path. which is appearing with Error Code :- 1905
C:\Program Files (x86)\ABB Symphony Plus\Engineering\Composer Harmony\bin
1. ComposerConfigDataX.dll
2. ControllerConfigDataX.dll
3. ControllerConfigViewX.dll
4. DataBrowserX.dll
Can anyone suggest us what is the issue and the solution to fix the same.
Answers
What is the Windows versions and is it x64? From the release notes Composer 6.1 only support x64 Windows versions. Please check release notes as there are other issues to do with account names and so on. Docu: 2VAA002088-620
Add new comment