Aspect View Wrapper
Is there any way to dynamically assign the view reference for an Aspect View Wrapper in PG2 graphics? I have v5.1 sp2 and have tried using different view references in an if statement based on a local variable, but it does not trigger the aspect view wrapper to change it's view reference when the variable value changes.
Voted best answer
Thanks, I imported it to a FP4 Rev. D system. When I set the button to Area, the view does change to Aspect 2, and when I set to Status, it switches back to Aspect 1.
When I went through the fixed problems section of FP4 Rev. D, I noticed that two fixed problems on pages 41 and 70, Rev. D and Rev. A respectively, match with what you experience. However, I was not able to find a workaround without upgrading. Please see 2PAA111288-510 for relevant information: http://tinyurl.com/l4qojcs.
Answers
It should change indeed. Can you possibly attach an export file?
Add new comment