Update the Firmware in PM554-eth
Hello Team,
I download the Firmware file from the ABB Site.
what is the procedure to update the firmware in PM554-eth through SD card.??
What we have to change in .INI file also.
i want to update from 2.5.1 to 2.5.4.
Answers
Hi,
PFA the document which describes the firmware update procedure using an SD card.
Note:
In case you are using newer versions of automation builder, you could update the firmware directly from Automation builder, by logging into the CPU>> Firmware info>> Select the device to be updated from the list and click on Update button located at the bottom of the Firmware info page.
This will allow you to update the firmware to the version available with the installed automation builder software in your PC (Firmware files located at C:\ProgramData\AutomationBuilder).
Use the SD card method if you want to update to a firmware other than what is available in your AB installed PC.
Regards
Rahil
Hi,
During a power ON boot of the PLC with the prepared SD card inserted, only those components' firmware will be updated, against which FirmwareUpdate in the .ini file is set to 2 or 3 and FunctionOfCard=2 .
Regards
Rahil
Add new comment