Faceplates isn't working.
I have created a project with PCIT FBs and want to crontrol them through faceplates. But I do not get them to work. I have downloaded the program from control builder to the cpu and i can force the tags, but i want to test the faceplates but they are dead. What do I need to do to make them working?
Answers
Which control system 800xA? which controller AC800M?
If 800xA with AC800M did you add the controller to the opc server?
Check OPC Data source definition.
Solved
by MRHY Rank: 4528 on 12/7/2017 6:20:57 AM | Like (0) | Report
I am using 800xA and AC800M
Add new comment