Hello, i can't load VIS to the emulator; the cause is that there is no tcp/ip connection, please help me
Answers
Greetings,
Have you ever create a new controller via internet explorer?
Web adresses is http://127.0.0.1:8888
If you did not create any controller, VIS emulator could not recognize it.
Hope this helps.
thanks for your answer, yes i create a new controller, i can load the proces station D-PS but i can't do it for the operator station. in the beginning i did it but after have made modification it hase been impossible to download it a other time.
Hi again,
If you have started the Digivis, you can load VIS to emulator. But you have to configure Resourse ID and IP Adresses correctly.
Hope this helps.
VIS should be a PC, can't a emulator.
And make sure your PC is connected to any LAN/Internet.
otherwise your Digivis station will show "no connection" in CBF tree
Add new comment