XenServer Virtualization and distributed aplications managements runs over 800xA???
I am looking information about multi-site sinchronization to operate remotely several facilities from a central center ensuring operational continuity of local sites when any connection failure arise with the remote center?? Citrix XenServer (used in critical IT applications), promises to solve this kind of problem while minimizing the loss of service. ABB recommends this type of technologies or ABB have they own?
Answers
Haven't heard that ABB have something similar to the Citrix XenServer.
ABB recommends to use Microsoft Terminal Server for the 800xA remote clients (rich clients). In 800xA earlier than v5.0 Citrix Metaframe was used as a solution.
There is also question regarding functionality side (pro&cons) - see attached file (screenshot).
Add new comment