AC-70 function chart builder
Hi,
I am using an AC-70 controller.
Using
Application builder 4.1/0
Bus configuration builder 3.0/1
Function chart builder 6.2/1
Online builder 3.0/2
Now i have a program in function chart builder of version 4.6/1.
It is doing some problem because of version mismatch and i have only 6.2/1 version. So i want to change the program version from 4.6/1 to 6.2/1.
If it is possible then please give me procedure.
Answers
Go online with the old FCD to make sure you have the same version program. Create controller in new application builder. Create source code from database and pc program with the old version FCB and backtranslate this in the new version FCB. Download with new version FCB.
by BR Rank: 359 on 12/5/2017 12:12:09 AM | Like (0) | Report
If version change is not possible then give me any way that i can open the the program of 4.6/1 in FCB 6.2/1.
Add new comment