DSTD N020 ERR Indication LEDs are RED
What does the ERR LED means on DSTD N020 Connection Unit. These are steady RED at the moment but the output is in normal state without any alarm. What does this means and how to extinguish this ERR Led.
I have read the manuals and it was mentioned that "The current in the loop must exceed 125mA to extinguish this LED".
Answers
Hello,
Please check the mmcx messages of SideA & SideB controller it will give you the hint to resolve the issue.
May be channel may be fault in any of the controller.
Add new comment