Trend not showing
whenever i open trend display i then see the trends starting to build up. i want to see trends to be continuously recorded. So that if i want to see trends before an hour i can open the trend display n see or even earlier than that. Im at site . CompacT hmi 800 5.1. This is my first chmi comissioning. Please help, i will be grateful to you.
Voted best answer
You mean that right now when you open up the trend you can't see any previous data?
A trend itself doesn't store any data so if you open up a trend it will start to display new incomming data which will be lost when you close it and open it again.
To get the trend to keep and be able to show previous data you would need to set up a "log configuration" to store the data so the trend can display previous values from the log.
Add new comment