I'm working with PM866 controller and I need to know why it's heap utilization increase (800XA 6.02)
After application download the heap utilization was about 40%. But in this moment, after seven days, its has 82%.
I attached the controller logs that can help to review this extrange behavior.
Thanks in advance for your help.
Answers
Hello,
We have faced simialr issue with 800xA V 5.1 (Base). We segregated the Network Switch and then only issue got resolved. At my end, not sure this is only the reason but issue got resolved. You can try once by segregating CN & PN is different switch.
Regards,
Shiv Kumar
by ecofre Rank: 943 on 1/12/2018 5:23:17 AM | Like (0) | Report
Hi,
I used the Heap Statistics tool and I found that the PhDrvHndl ElementType cause the heap utilization increase.
Somebody know wath is the function of this element?
Thanks in advance!!
Add new comment